Hello, I want to realize up-conversion at 250MHz and 350MHz using DAC38J84EVM with NCO. The following screenshots is my configuration parameters in DAC3XJ8X GUI v1.1 and TSW14J56EVM. After click the "Updata NCO settings", the actual NCO setting become "FFFFFFFFF" and there is no output. I wonder what is the problem and what is the procedure for up coversion with the GUIs. Besides, how can DAC38J84EVM can achieve 1GHz of bandwidth ? Thank you.