Hello there,
I have a customer who reached out to me with a question regarding the on-chip tuners internal to the ADC32RF45 (DDC Block) and they're looking to understand the correlation between the multiple data rates (output from device over JESD links) and different decimation settings as they're developing the DSP code in their FPGA.
He is planning to use the device in receiver mode while using two bands. Please see his question below--
'In looking at the datasheet for the device, I see that table 3 on p.34 describes output rates and bandwidths based on the sample rate for various decimation settings and it seems pretty straightforward. However, when I look at Figure 76 on p.35 which gives an example of a dual-band divide by 8 complex setting and try to reconcile the numbers shown in the figure with Table 3, things don't match.
The figure shows that the complex output data rate is 750MSPS per band for divide-by-8 and a sample rate of 3GSPS, while table 3 shows that the rate should be 375MSPS per band complex for the same sample rate. There is a factor of two discrepancy and I'm wondering if there is either a mistake in the figure or perhaps I am not understanding something (like does the rate in the figure refer to IQ pair rate, while the table refers to individual IQ stream rates which are presumably interleaved)?
Can you shed some light on this?'
Appreciate any feedback your team can offer us! Thank you for your time.
-Amanda