Hi All
I have two LDC1000 EVM and I was testing them with LDC1000_EVM_GUI_1_0_2_0, all was (quite) fine.
I have installed LDC1000_EVM_GUI_1_0_4_1, but now I have big troubles in working with it.
I upload the firmware with “LDC1000 Firmware 0x300.txt”, switched the driver, installed and re-installed the GUI but:
- The driver seems works fine, I can use Hyper Terminal for talking with the LDC1000 EVM in reading and writing mode.
- When I start LDC1000_EVM_GUI_1_0_4_1, I can update the LDC1000 EVM firmware, I can see the resistance values on the diagram, and switch the LEDs ON and OFF, but, when I try to modify some parameter like Rmin, Rmax … ( after I stopped the acquisition), no modification is made and the GUI does not run anymore.
I also tried to switch back to LDC1000_EVM_GUI_1_0_2_0, but I got no connection with the LDC1000 EVM ( I suppose the new firmware is no working with the old GUI).
Any idea? Can I switch back to the old LDC1000 EVM firmware and use GUI_1_0_2_0 that at least was (quite) working ?
Thanks
VT