Hello
I now try to use two EVMs simultaniously. I observe that the data are affected when they are approximately 5 cm and closer apart. Is the data still realiable (non correlated) or are they correlated?
The data is affected more the closer the coils are.
I wonder how this will affect Applications With more coils for temperature Independence or "Lateral position sensing with z-axis insensitivity"
What I saw in my trails was that even if the coils had fixed distance the samplevalues decreased at some distances even if the coil traveled towards the metal Object. And the noise could be huge and/or uniform.
Regards Torgeir