Hello,
I'm currently evaluating the LDC1000EVM.
Target is the sphere with which only the surface was metal plated ware. (3mm in diameter)
I'm looking for a way to increase the sensitivity.
Do you have any good suggestions?
BR,
Seishin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm currently evaluating the LDC1000EVM.
Target is the sphere with which only the surface was metal plated ware. (3mm in diameter)
I'm looking for a way to increase the sensitivity.
Do you have any good suggestions?
BR,
Seishin
Hi Don san,
Thank you for your response.
The following information that I have.
Plating thickness : 1 to 5μm
Plating materials : Electroless nickel plating
Float ball diameter : 5/32"(3.97mm)
Tapered tube : PYREX,66mm(H),φ9.5mm
Best Regards,
Seishin
Hi,
The Eddy current requires at least 30um of metal. Since the plating is much thinner than 30um, the sensitivity will be very poor.
To increate the sensitivity, you may try a wire-wound coil circulating the tube. This can improve sensitivity significantly.
Best regadrs,
Don