From what I can tell, the ADS79250 family uses SPI mode 0, since it latches input data on the first clock edge, which is a rising edge. The data sheet says it supports a 20MHz SCLK for 3V VBD, but the td2 max delay is 27, which means the SDO may not be valid on the rising 20MHz SCLK edge, requiring you to sample it on the following falling edge. Since SDO changes a set time after the SCLK falling edge, you could sample SDO on the falling edge, but that would mean the ADS is not operating in the same SPI mode as the master device. So can I just use SPI mode 0 for both as long as I have a 14MHz clock or slower, and set the CS related delays?
Thanks,
James