I jsut bought a ADS1282EVM-PDK and followed the manual to use it in ADCPro. http://focus.ti.com/docs/toolsw/folders/print/ads1282evm-pdk.html
However, when I tried to load the EVM plugin in ADCPro, I did not see message window for installing USBstyx as stated in 10.2 Fig. 17 in the user guide. Then I got time out error and "DSP is not ready" msg in ADCPro. Meanwhile, only 4 segments of the 8 segment LED on the MMB0 DSP board are lit. Check the WINXP device manager window of winxp, only see NI-VISA entry, no USBStyx. Looks like the DSP fw can not be launched correctly. Either the bootloader is wrong or the fw is wrong. The MMB) board is TMS320VC5507 dsp based. Can anyone help me to figure out what's wrong?
I have already sent the help request to TI technical support for more than two weeks and call them a couple of times, but the only reply is they can not provide the assistance at the moment and suggested me to try this site.
I use this evaluation board package to speed up my evaluation, but now I get stuck here and can not get any useful response from TI. Can anyone help me, thanks lot.