Hi,
I have two questions about operation of AMC7812 EVM.
1.
I didn't provide any signal including GND to ADC channel but the ADC-n-data registers have these values.
You can see above figure. Is it normal operation of AMC7812 EVM?
2.
And, 0x666 value of ADC-15-channel is supplied by DAC-1-channel with loopback configuration of AMC7812 EVM.
But the 0x666 value are fluctuated when the ADC-14-channel is enable. ADC-14-channel connected with GND.
And, ADC-13-channel is odd value as you can see above figure.
How can I fix it?
Best Regars,
Seung Joon Lee