Hi all,
I'm currently evaluating the ADS1247 and I want to test the SPI interface without dealing with the ADC part for now. I'm using a BeagleBone Black (BBB) as the SPI master. Is it enough to connect the ADS1247 like follows?
- DVDD -> +3.3V
- DGND -> GND
- SCLK -> 1MHz @ BBB
- DIN -> MOSI @ BBB
- DOUT -> MISO @ BBB
- CS -> CS @ BBB
Do I also have to pull RESET to GND? What about the START pin?
Thanks for your help!
Best regards,
Simon