Hello fellows,
I am having trouble with the commissioning of the ADS1256, I already asked the supplier and other communities but so far nobody could give me a proper answer, so I hope that you guys can help me out.
I have the ADS1256 setup on an sensor board together with an analoge sensor, the sensor board itself is working fine as I bought it from a supplier that also provides a software, and its working. Now I am trying to create the spi communication on my own, using the arduino but the ADS1256 is not answering at all. I have tried alot command orders but I do not receive any converted data.
So I am no really sure if the order of the commands that I send are correct, so my question is if anyone can provide me correct order of the commands that I need to send to the ADS1256 in order to receive data. Especially which commands do I need to send only once (as initialization) and which commands do I need to send constantly (within the loop).
An Arduino exampel would be perfect but I am happy with any other source code or help I could get.
Thanks alot in advance!!!
P.S. sorry for my bad english:)
Regards