I have two questions when I try to use this IC(ADS7850).
As you know, generally speaking an ADC will have two stages, one is conversation stage to convert analog data to digital data, and another stage named acquisition stage which is to shift the digital data out through serial or parallel interface. Both those two stages need an SCLK. So my first question is can I use two different frequencies SCLK in the mentioned two stages respectively, such as I will involve an 20 MHZ for conversation stage and 15MHZ for acquisition stage. Will this behavior bring some potential issue to the ADC?
The second question is: what is the setup time from SCLK falling edge to the output data valid? I can only find a items that setup time from SCLK falling edge to previous data valid, but this will not make sense. I need to know the time from SCLK falling to current data valid.