Hi all,
I'm now testing the ADS8881EVM board due to the reference design and datasheet. And I have several questions as below:
1. As the input anti-aliasing filter design, make the Cfilter >20 Csample (page 8 of the ref design), it said it's a rule of thumb. and I wonder how does this rule derive?
2. Similar question with 1, Rfilter should be 20 times smaller than Rswitch (page 9 of ref design), how does this derive?
3. The ref design is to achieve a SNR of 98dB. However, my result is only 96dB. I found that, when calculating the system noise, the ref design doesn't count the noise of buffer at reference driver. I found it might be large without a filter at output. when removed it, test result of SNR increase to 97dB . So I wonder whether I should use a buffer at ref. I know it can offer larger current output for ADC ref, but it also increase noise. Could you tell me how can I balance these two effect? Or how can I calculate between these two situation before test. For this case, just a REF5045 with a low pass RC filter (large capacitor) is better.