I'm incorporating sensors into a robotic finger. The microcontroller in the palm has 4-wire SPI capabilities but doesn't have any extra I/O pins available for separate slave-select lines; I need Daisy-Chain communication between ADCs on various phalanges/fingers. We are tight on space, so a 4-channel (or more) IC with high analog input impedance/buffers incorporated would be ideal to reduce the number of components. Resolution is less important than sampling speed.
I found the preview datasheet for ADS8684 and it seems just right. Is there an alternative ADC chip that might fit my application?
Also, if an ADC chip does not specify that it has a Daisy-Chain mode is there any way to implement daisy-chaining anyway? Somehow access the I/O shift register directly when the SS pin is not active to pass-through messages?
Thanks!