Hi, i have the DAC161S997EVM and want to install the DAC161S997GUI from here http://www.ti.com/tool/DAC161S997EVM (red Download button).
Installation of the Programm and the USB-Driver of the FTDI-Chip works under my Win7-Pro. When i connect the board to the PC i can see the new COM-Port in the Devicemanager. But when i start the DAC161S997GUI, i get the following error:
Error -1073807202 occourred at VISA
Can somebody tell me which driver i need for this? I red that VISA has something to do with LabView but i dont use it.
Regards Andre