Hi there
I'm working with an ADS8319 ADC. The attached picture shows the part of the scematic where the ADC is located. REFIN is a reference voltage of 4.096V. So it should be possible to sample values between 0V and 4.096V at the analog input pin, right? But if I go up to about 2V at the analog input pin, the ADC already shows me a value of 65536 on the SPI data line. Why can I only use half of the value range I want to see? Any ideas?