Hello,
What are the verbose CLK Input Pin requirements for this device, apart from the frequency capabilities and requirements that have been well-defined in the datasheet? (ADS1278-HT SBAS447E –MARCH 2009–REVISED APRIL 2013)
Specifically,
- What voltage levels is this pin expecting to function correctly and avoid device destruction? 0-DVDD or 0-IOVDD...?
- Does this pin expect a standard CMOS clock input?
- What duty cycles are recommended to maintain conversion accuracy of the chip? Would a 55/45 CMOS signal be compatible, or should this signal be manipulated to ensure 50/50 duty cycles?
- What relevant pin/circuitry parasitic should designers be aware of, apart from the recommended 50Ω series source termination already identified in the datasheet? (eg, input impedance/bias currents, input capacitance, internal pullup/downs).
Thank your for your assistance,
-Andy Gauvin