Sorry in advance for this question with possibly obvious answer. I have two input signals that I'd like to measure with single ADS1120. First is strictly unipolar in the range of 0 to 2.5V and another bipolar (range: -0.2V to 2.5V). I'd like to use external reference REF5025 and don't need any amplification therefore PGA will be disabled with gain set to 1.
Please let me know is it possible to do that with single device? In that case I presume that AVSS should be below zero (i.e. -2 to -2.5V to be within allowed limitations). I didn't find a single reference in datasheet about measurement with AVSS bellow zero. I'd like to use +5V for DVDD.
Many thanks in advance.