I'm implementing impedance measurement and have some questions. I have read many posts and documentation but still coudn't get around some issues. Specifically, at Figure 48 from ADS1299 datasheet, I need to know which switches are closed for different lead_off configurations.
1) The selected current magnitude, corresponds to mean value at DC excitation and peak-to-peak at AC? I can't find this info on the datasheet.
2) At the figure below, Config 1 and 2 correspond to which models?
3) The example at page 38 of SLAU443, corresponds to which configuration for LOFF_SENSP, LOFF_SENSP, and which model A,B,C or D?
4) The model E is supposed to be the circuit used in the mentioned example. The documantation says 120 mVpp = 2 x (6nApp x 5kohm + 6nApp x 5kohm). which is the return path for excitation current? why does it multiplies by 2?
Thanks in advance
Leo