Hi,
I bought an ADS1201 Delta-Sigma modulator for a medical applications. I'm trying to reconstruct the analog signal that enter to the device.
The input signals on the modulator have frequency that start from DC to 100Hz and have an amplitude from 0 to 5V. The output 1 bit stream of the modulator have frequency of 1MHz (the clock of the modulator).
After the modulator should be included a digital low pass filter which acquires only the useful signal and discards the quantization noise, in cascade a decimator to decrease the frequency and increase the number of output bits.
Exist an IC that I can connect in cascade of ADS1201 and obtain the 24 bit signal?
After that I have to reconvert the 24 bit to analog signal. What model of IC I can use for this operation?
Thank you in advance.
Riccardo