I bought a DAC1220EVM module and want to evaluate it using the DXP software. Can I just buy another ADS1262EVM-PDK and use the MMBO motherboard for evaluation of the DAC1220EVM? I don't see a way to just get the MMBO and there is no DAC1220EVM-PDK available at least as far as I can see. I don't want to hook up the DAC1220 to the MMBO I got with the ADS1262 with out understanding if it might damage one or both as I don't know if the MMBO is generic.
I went through the schematics for the MMBO rev D and did not find a show stopper for hooking up the DAC1220 so I did with no results. Also when I run DXP it brings up the DXP DAC Config File Downloader and show multiple DACs but when I try to download any of them I get an error pop up that says it was unable to download file XXX.xml. The green light indicating internet is working but no banana. I also tried to scan for devices and it shows nothing. The ADCpro works fine with the ADS126x EVM module.
I googled DAC1220.xml and found it using google.
I copied it to the device directory and the program runs with it so far. The down loader seems to be not working on my win7 64bit professional operating system.
What I found is that the program runs but is not communicating with the device or the MMBO as configured. How do I get this thing working? The driver shows up in the device manager but I keep getting USB Connection time out and no communications. ADCpro works no problem so what is the problem with this and is it because the MMBO for the ADS1262 will not work with the DAC1220?
Any help would be appreciated.
Best Regards
Peter