Hi,
I´m making a design consisting of 4 ADS1255 (high resolution converter). The 4 ADC shall be synchronized why I need to feed them with the same clock signal. One idea was to connect one crystal to the first ADC and use the output signal from this ADC (CLKOUT) and connect it directly to CLKIN ports of the other ADC´s.
Would this solution work?
-CLKOUT signal quality good enough to feed CLKIN?
-Does CLKOUT generate enough current to power the CLKIN of all 3?
If the answer is no, do you have any suggestion of suitable external clock generator for the ADS1255?
Thanks for your help!