I’m using the ADS 8028 to read several signals in my circuit. One input (AIN6) is from a voltage divide, which accepted its voltage from a DAC.
The reading of that input is offsets by ~70mV , by unknown reason. I have to emphasize, that I measured ( with DVM) the voltage in the ADC input, and compared its value to the read value by the ADC. All the other inputs is correct. There is one input which tied to GROUND, and the reading of the ADC is also correct(<1mV).
Following a graph of the measured input versus the reading values:(The Y axis is millivolts)
The ADC operated from external reference, which is its the supply voltage- 3.3Volts
This is the ADC circuit:P2.PDF
The source for the AIN6 input( through R15) :P1.PDF
Do you have any idea ?
Thanks
Shlomo Perlshtein
Board Designer
Elbit Systems Ltd.