Hello, I have integrated an ADS1158 into our product and the setup is as follows:
-Unipolar operation
-External ADC amplifier (OPA2365 buffer external to the part) - Bypass bit = 1
-START = LOW
-Configured for scanning mode (not fixed channel)
-DRATE = b11 (23739 SPS)
-Using pulse convert command through SPI to trigger measurements
Here's my question / issue:
The timing from pulse convert command transfered to DRDY line low = 40.4uS consistently.
No matter what I set the DLY bits to there is not change in this timing. I would expect that a DLY of b111 would cause a much slower measurement cycle and allow more settling time.
The reason I am asking is that I may consider removing the external buffer amplifier, but then I would need the additional settle time. I tried setting bypass to 0 and DLY still had no affect on the timing of DRDY.
Thanks for your help.