This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: Deboxing the DAC161S055EVM

Other Parts Discussed in Thread: DAC161S055, DAC161S055EVMHello, today I received my DAC161s055. Unfortunatelly after 5 hours i found tha the document "firmware “dac161s055_fwv0.89.
.txt" is not present in the download. Insteasd there is THE DAC 12xSXX. seems like the files are mistaken.
We need sombody to fix it


Thank you Pablo
  • Pablo,

    I split this and moved it to the Data converters forum since MSP doesn't actually make this EVM - hopefully the team there will be able to better help you. Thanks for providing feedback!

    -Katie
  • Hi Pablo,


    After downloading the software (snoc021.zip) unzip the file and install the software.  If you use the default installation location the file will be in the

    C:\Program Files (x86)\Texas Instruments\DAC161S055\Firmware

    directory.  It will be called: dac12xSxxx_fw-v0.87.txt

    Mike

  • Dear Pablo;

    If I remember correctly, there was an error made with regard to a file name in the TI *.pdf literature and the correct file name that you see when you download the TI program. I made two posts about deboxing the DAC161S055EVM. I will try to provide you with a link to these discussions when I locate that link.

    I had a lot of problems with this kit.

    I have found the start up kit programs to be difficult to work with.

    Tell me if you detect a lot of current going to the ground pin of your oscilloscope (arcing).

    If you do not own an oscilloscope, the probability that you will get this kit working in a time efficient manner is very, very, poor. Better documentation - standalone working programs - are needed.  When I use the term "standalone" program, I mean a program that does not require to be interfaced to a GUI or any other interface - a simple program that downloads directly from the CCS IDE to the Launchpad and as a result the booster pack works - no other program necessary.