Hello,
I am using the ADS1220 to measure two different signals in a system with Vref=AVDD=2.7V. Both signals are ratiometric.
One is a truly differential signal centered at AVDD/2, which is read 250 times per second (and has an internally set sampling rate of 1000sps to enable this)
The other signal is an NTC thermistor with resistor divider, so the Vout can span from 0.07*AVDD to 0.9*AVDD. Once per second, I switch from the former to the latter, take a single shot measurement, and switch back. There is a delay/gap in the first measurement due to this switch, but so far that has not been a problem since we only read the first signal every 4ms. So, I have two questions:
Due to the single-ended thermistor violating common mode voltage limits, I have to consider the following:
1. Is there any switching or settling time associated with disabling and enabling the PGA? What about changing gain?
2. Can I set AINN to be a system monitor voltage, i.e., AINN = AVDD/2 and AINP=Vout of thermistor? Other threads I've read on this forum list single-ended signals as referenced to AVSS, but is there any issue with measuring it pseudo-differentially against an internally-derived system voltage?
Thank you for any advice and input you can offer,
Kevin