Hello,
I would like to confirm the program sequence for Auto-1 mode continuously. (repeat the conversion CH0 --> CH1 --> CH2 --....--> CH7 --> CH0 -->CH1--> CH2...CH7-->CH0-->.....)
(1)
Is the following program sequence for above operation correct?
1.Device Power Up
2.Device Operation in Manual Mode as default
3.Set the mode-control register of the Table 2 for Auto-1mode
Then change to Auto-1mode
4.Set the program register of the Table3.
5.Set the Continued Operation in a Selected Mode of the Table 7.
Should we set the table 7 for repeating operation?
(2)
Regarding Table2 DI10.
According to Figure 52, I understood that we don't need to set the DI10 of Table 2.
Is my understanding correct?
If yes, when should we set the DI10 to "1"?
Best Regards,
Ryuji Asaka