Other Parts Discussed in Thread: ADS1298
Hello everyone:
I am making a 40-ch EEG sampling system using five pieces of ADS1299s and one STM32 ARM. I want to configure the five ADS1299 in Daisy-Chain mode but I have some questions to be solved
1. When configured in Daisy-Chain mode, can the five ADS1299s work in internal or external clock mode separately or must they work in the same clock system? I see someone configure the first ADS1299 working into internal clock mode and output the clock to drive the other four ADS1299s. If the working mode is correct? I am afraid that the clock wire go across the board and has electromagnetic inference on the other chip on the board.
2. In Daisy-Chain mode, the 5 ADS1299s share the same /CS, START, RESET, SCLK and DIN signal, how to configure all the registers? How can we read and write the registers of different ADS1299?
3. Someone posted in the forum said that there is must a SCLK between the data of two ADS1299s, but I look up the chart of Daisy-Chain Timing in the manual, it doesn't mention that. Is it necessary to add a SCLK between the two ADS1299 data?
Thank you very much.