Hi,
We have used THS8200 in our custom board design and we are facing a strange and very rare issue. In our design DM8148 DVO2 output is provided to THS8200. We are using standard driver provided with DVR-RDK-4.1 to configure THS8200. We are successfully able to configure it for almost 15 resolutions and everything works.
We have developed 250 board but on 9-10 board we are facing strange issue. With same binaries we are observing that on these boards no output comes from THS8200. We don't see any activity on R, G and B lines also we are not seeing Vertical Sync signal and only Horizontal Sync signal is available but with wrong frequency.
We have measured the sync frequencies and pixel clock frequency at the input side of THS8200 which is output of DM8148 and all these signals are OK with respective frequencies.
We are puzzled that where is the problem because on ~240 board everything is working. Chip assembly seems OK as per our observation.
Can anyone suggest where we should look into to solve this problem?
Thanks,
Ronak