I understand that the BT.656 super-frame that is build consists of video lines each of which has a unique identifier defining the source and line number. Also, I understand that the nature of the asynchronous inputs necessarily means that from time to time dummy lines with no video will be inserted. To this I have the following questions:
1. The TVP has to sense vertical sync for each of the four inputs separately. It seems to me then, that the line number that appears in the super-frame for one input can be radically different than the line number of the next line that represents a different input. That is, it is possible for two consecutive lines to appear from input A, B to have, say line number 25 for A and line number 286 for B. Is this so? If so, then the video input processor has to carefully build each of the four input fields from this information and that the asynchronous nature of the input are maintained, i.e. only lines are synchronized but not fields or frames.
2. Is it possible under any circumstances for video lines to be lost, say during the output of dummy lines?
Thank
Michael Stamler