This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150: TVP5150

Part Number: TVP5150

Dear Sir,

We have requirement to interface 1" 2" LCD on PAL input .

We have located LCD which has 8 bit data or 16 bit data input.

Please let us know can we connect the TVP5150 output to LCD??

Any agency you can suggest  who can provide us the solution?

you have any EVM for TVP5150.?

Regards

Seema Joshi

3 Replies

  • The TVP5150 will digitize analog PAL or NTSC video and output a corresponding ITU656 digital stream. If the LCD can accept ITU656 video directly then you can use it. You will need to contact your LCD manufacturer for more information regarding the input formats supported.

    In general though, I doubt you can connect directly to the LCD since most LCD displays accept progressive video formats but PAL/NTSC are interlaced.

    BR,

    Steve

    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

  • In reply to Steve Clynes:

    Hello Steve,

    Need your help design & development with the chip TVP5150.

    can you provide schematic as well as design files for the same? as well as arrange samples?

    Regards

    Seema Joshi

  • In reply to seema joshi:

    Unfortunately all that is available is what is in the datasheet.

    BR,

    Steve

    Please mark this post as answered via the Verify Answer button below if you think it answers your question.  Thanks!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.