This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Customer got a question about the compatibility design for the LP8556SQX-E08/NOPB and LP8556SQX-E09/NOPB.
The E08 version default channel number is 4 while that of E09 is 6.
1. Could we set follow EPROM setting of LP8556SQX-E09 and change the LP8556SQX-E08 register using I2C to enable 6 channels?
2. If we can make the LP8556SQX-E08 enable 6 channels. We should reprogram LED_EN bits to change LED string counts enabled and set PS_MODE bits accordingly ,right ?
3. To reprogram the register , we should power up the VDD and not enable the EN/VDDIO , right ? As the config registers are not accessible in the Active Mode
.
Thanks!
Reagan
Hi Reagan,
1. Could we set follow EPROM setting of LP8556SQX-E09 and change the LP8556SQX-E08 register using I2C to enable 6 channels?
Yes you can write the value in register A3h and A5h when powering up to enable 6 channels for E08 version.
2. If we can make the LP8556SQX-E08 enable 6 channels. We should reprogram LED_EN bits to change LED string counts enabled and set PS_MODE bits accordingly ,right ?
LED_EN bits are default as 1. These bits are AND with the internal LED enable bits that are generated with the PS_MODE logic. So only change PS_MODE bits is OK.
3. To reprogram the register , we should power up the VDD and not enable the EN/VDDIO , right ? As the config registers are not accessible in the Active Mode
EN/VDDIO is the power supply reference for interface pins. So it need to be enabled before writing I2C commands. You could pull PWM input low when reprogram the registers.
Hi Hardy,
Thank you so much for your quick response!
For the "pull PWM input low when reprogram the registers" , you mean pull the 9pin low so that there would be no output , right ?
Hi Reagan,
Yes number 9 pin. For 'PWM only' version, BL_ON bit is default enable so that PWM input would drive outputs directly.