This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8556SQ-EVM: LP8556SQX-E08/NOPB

Part Number: LP8556SQ-EVM


I am trying to use this part to an existing system.  I am wanting to use it with out PWM and I2C.  I just want it to maintain a constant 50 mA on our back light for 3 arrays of LEDs.   I believe this can be done in manual control.   The Iset in the data  sheet is linked to the I2C and does not set this value.   If the voltage in my circuit goes too far over the 30 Voltage we could damage our Backlight.  What does this part do if the i2c is not used.  For the PWM I was going to pull that value high.   Diming is not to be used in this design.  What value of Iset will do this?