This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gents,
Congrats on the good progress on CCSv5.1!! Keep up the good work.
I have just installed v5.1.0.08000 (yes, I am a glutton for punishment...:). When attempting to build one of my DSP/BIOS projects I get a build error saying that the project was created with a version of DSP/BIOS tools that is not installed. I then installed DSP/BIOS v5_41_07_24 in the same directory as ccs (C:\ti\ccsv5 & C:\ti\bios_5_41_07_24). However, CCS does not auto-discover the DSP/BIOS install, and I cannot figure out how to manually install it. Can you give me some guidance?
Thx,
MikeH
Hi Mike,
Can you check the BIOS search paths (Windows->Preferences->Code Composer Studio->RTSC->Products) and see if the root location you installed BIOS shows up and also check what shows up under the 'DSP/BIOS' listing for 'Discovered tools'?
Thanks
ki
Hi Mike,
You are correct. M8 does have issues with BIOS installs that it did not come with. We are looking into this. In the meantime, there is a workaround you can use. You can delete (or cut and paste somewhere else) the 'eclipse folder inside the BIOS install (.\bios_5_41_07_24). Then restart CCS and it should detect it.
Thanks
ki
It is in the root directory of the BIOS install.
ex:
<INSTALL DIR>\bios_5_41_07_24\eclipse