I have 2 questions regarding CCS5.1
1. How to install ivahd netra simulator on CCS5.1? There a pdf ivahd_installation_steps_on_ccsv4.pdf which gives the complete idea of installation on CCS4.2 and is working fine. Is there any such pdf for CCS5.1 too?
2. I run one GEL file on CortexA8 on CCS4.2 for the initialization . Doing that I later could connect to CortexM3 and other ARMs . The same GEL file when I run on CCS5.1 it does not run and exits with error. What is the difference between running this GEL file on two different CCS versions? I use Netra target configuration on CCS4.2 and TI816x on CCS5.1.
Please help.
Thanks & Regards,
-Viranjan