This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use the Profile Clock for C55x.



How to use the Profile Clock for C55x.

I want to see the right usage of the Profile Clock.

I am using TMDX5535EZDSP in CCSv4.

CCS menu to enable the Profile Clock is "Target - Clock - Enable".
CCS menu to reset the Profile Clock is "Target - Clock - Reset".

I used the Profile Clock in two case for the following assembler cord.

       mov hi(ac0),*ar1 || mov ac0,*ar3
       mpym *ar0+,uns(*ar3+),ac0
       macm uns(*ar0+),*ar1+,ac0
       macm *ar0+,uns(*ar3+),ac0
       macm uns(*ar0+),*ar1+,ac0
       macm *ar0+,uns(*(ar3+t0)),ac0
       macm uns(*ar0+),*(ar1+t0),ac0
       macm *ar0+,uns(*ar3+),ac0
       macm uns(*ar0+),*ar1+,ac0
       macm *ar0+,uns(*(ar3-t0)),ac0
       macm uns(*ar0),*ar1,ac0

       amov #PreEQCoef1,ar0
       asub #5,ar1
       macm *(ar0+t0),*ar1+,ac0>>#16
       macm *(ar0+t0),*ar1+,ac0
       macm *(ar0+t0),*(ar1+t0),ac0
       macm *(ar0+t0),*ar1+,ac0
       macm *(ar0+t0),*(ar1-t0),ac0
       sfts ac0,#2       || mov #4,t1      
       sat ac0

       mov hi(ac0),*ar1 || mov ac0,*ar3

The first case, I put a breakpoint in the first line and the last next line each and ran the program.
When stop at the breakpoint of the first line, I reset the count of the Profile Clock.
When stop at the breakpoint of the last next line, I watched a result, it is 24.

The second case, I run the program by single-step.
When stop at the first line, I reset the count of the Profile Clock.
When stop at the last next line, I watched a result, it is 21.

Why is it that results were different?

Best regards,
Daisuke