This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C55x profiling tools missing in CCSv5.1.1

Hi John

Just installed the v5.1.1.00031 into my 5.09.xxx version and the all the profiling tools have gone ? I'm (was) using the C55xx v3 cycle sim to profile functions for a C5515.

How do I get it back ?

Cheers

Jon

  • Jon,

    I installed 5.1.1.00031 and I still have access to profiling on the C55x v3 cycle accurate simulator.

    I am able to set it up and get results.

    Are you not seeing the profiling menu items on the Tools menu?

    Regards,

    John

  • Nope, I've just removed the 5.1.1 and re-installed 5.09.xx version

    I may try to install the 5.1.1 in parallel and not into the 5.09.xx version later.

    Where can I find documentation on all the new features in the c-compiler and asm tools ?

    The docs on the web are from 2003/4 and can't find info on many new fetures:

    ex. #pragma nnnn_MISRA or .cdecls directive

  • Jon Halland said:

    Where can I find documentation on all the new features in the c-compiler and asm tools ?

    The docs on the web are from 2003/4 and can't find info on many new fetures:

    The C55x Compiler and Assembler User Guides were updated and posted late last year. They are accessible from the links on this page.

  • Thanks for the tools link

    I re-installed the 5.1.1.1 in another dir than the xxx.09 version and the full tools menu is now available.