MCU: MSP430F5438A
CCS: v5.3
I've got 2 separate projects at the moment;
the first is for a normal MSP430 application, which resides in the main flash memory (0x5C00 onwards)
the second is for a custom BSL, which resides in the BSL Memory (0x1000 - 0x17FF). This project is based on the BSL found here.... http://processors.wiki.ti.com/index.php/Custom_MSP430_BSL
Both of these projects build and work separately, but I'm trying to create a single project in CCS that allows me to build separate binaries - with the ultimate goal of creating a single flash image that can then be converted into an MSPgangimage file.
The problem I'm having is that CCS seems to have a fixed one to one relationship with respect to a CCS Project and a Linked Image.
Does anyone have any experience of this?
Thanks in advance.