The CCS V5.5 Tool Chain Editor page displays the following messages in red color under Current toolchain: TI Build Tools
- "Orphaned toolchain com.ti.ccstudio.buildDefinitions.TMS470_4.9.exe.DebugToolchain.1531819188 (TI Build Tools)"
- "Orphaned builder com.ti.ccstudio.buildDefinitions.TMS470_4.9.exe.builderDebug.1982742727 (GNU Make)"
This problem occurred after checking out a CCS v5.4 project from subversion into a new install of CCS v5.4. The Used tools list was blank so I added ARM Compiler and ARM Linker without fixing the red error.
- Project->Properties
- Check Show advanced settings link at bottom-left
- C/C++ Build->Tool Chain Editor
My end objective is to fix a build environment problem that is preventing me from building
10:17:19 **** Incremental Build of configuration Debug for project selfTest ****
make all
Cannot run program "make": Launching failed
Error: Program "make" not found in PATH
PATH=[C:/ti/ccsv5/eclipse/jre/bin/client;C:/ti/ccsv5/eclipse/jre/bin;C:/ti/ccsv5/eclipse/jre/lib/i386;C:\Python27\;C:\Python27\Scripts;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files\TortoiseSVN\bin;c:\Program Files (x86)\Microsoft SQL Server\100\Tools\Binn\;c:\Program Files\Microsoft SQL Server\100\Tools\Binn\;c:\Program Files\Microsoft SQL Server\100\DTS\Binn\;C:\Program Files\Microsoft\Web Platform Installer\;C:\Program Files (x86)\Microsoft ASP.NET\ASP.NET Web Pages\v1.0\;C:\Program Files (x86)\Windows Kits\8.0\Windows Performance Toolkit\;C:\Program Files\Microsoft SQL Server\110\Tools\Binn\;C:\Program Files (x86)\OpenSSH\bin;C:\Program Files (x86)\VisualSVN Server\bin;C:\Program Files (x86)\QuickTime\QTSystem\;%APPDATA%\Python\Scripts;C:\ti\ccsv5\eclipse;]
10:17:19 Build Finished (took 39ms)
All tips and suggestions are much appreciated.
-Ed