I 'm using Code Composer Studio 6.0 .
I start working an old project and after the build that requires i see that have 10 errors .
I try to change the compiler version believe that fix the errors .
After the install the compiler 4.1.1 i see two errors:
1. gmake: *** No rule to make target `clean'.
2. This project was created using a version of compiler that is not currently installed: null [MSP430]. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of this version, or migrate the project to one of the available compiler versions by adjusting project properties.
I try to change from Properties the compiler version from 4.3.3 to 4.1.1 but Internal Error: java.lang.NullPointerException
What can i do to debug without errors and start working to the old project ??
Thanks