I'm writing some automation scripts that use DSS to communicate with my target.
So, I have to call DSS externally. Every time I open a session, it takes 5 seconds:
ds.openSession( "Blackhawk XDS560v2-USB Mezzanine Emulator/C66xx_0" )
and the console shows the message:
Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc
Is the probe really loading the FPGA every time I open a session? Is this causing the observed delay?
I need this script to run faster, because there are thousands of test cases to run on the target.
Any help?
Thanks.