Hi!
My config:
Host PC:
Kubuntu 12.0.4
alex@alex-GA-MA790GP-DS4H:~$ uname -a
Linux alex-GA-MA790GP-DS4H 3.2.0-67-generic-pae #101-Ubuntu SMP Tue Jul 15 18:04:54 UTC 2014 i686 athlon i386 GNU/Linux
alex@alex-GA-MA790GP-DS4H:~$
Target:
http://myirtech.com/list.asp?id=466
JTAG:
https://www.olimex.com/Products/DSP/Emulators/TMS320-XDS100-V3/
Code Composer Studio:
Version: 6.0.1.00040
Toolchain:
arm-2010q1 arm-none-linux-gnueabi-
I need to debug wifi driver, to do so, i've created a C/C++ makefile project with existing code in CCS. Then i patched the kernel (turn on "Compile kernel with debug info" and so on...), after that I’ve rebuilt the wi-fi driver.
The troubles starts then i try to load symbols from my wifi driver. After pressing OK button in the Load symbols window the CCS begins to load symbols, but crashes after a couple of seconds. There aren't any error messages or something else, just shutdown.
To find a reason of this i tried to rebuild kernel and wifi driver with another toolchain (i have arm-2010q1 arm-none-linux-gnueabi and arm-linux-gnueabi), to clear the CCS workspace and .ti folders, to create a new project, but result is the same.
But if i do the same steps with another driver (for example hdmi tda998x.ko), everything is ok and i able to debug it.
On the target side wi-fi driver is loading well in release/debug configuration.
Please see screen-shots and log files in attach.
Thanks in advance
Alex Grigoriev