I am attempting to use UniFlash 3.1.0.00026 on a 32-bit Linux VM to USB DFU a TM4C1233H6PM on a custom board. Please see this post for any additional info concerning the DFU problem: (http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/p/361329/1280318.aspx#1280318).
One method of approach to fixing our DFU problem was building our code image and installing it on a 32bit based linux system. I have installed UniFlash and its optional software. However, from the new target configuration the “Tiva LM USB DFU interface” option for connecting to the target is missing.
How can I add this connection type to my linux install of UniFlash?
-Matt