I followed the directions at http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS to install FlexLM. It gets to the final screen and shows "The installation of FLEXnet Publisher License Server Manager is finished, but some errors occurred. Please see the installation log for details." So, first I tried looking for an installation log...but can't find anything that looks like a log file. One would think that it should either be in the directory that lmadmin-i86_n3-11_9_0_0.exe was run, or in the install directory...but nothing.
I've spent well over 5 hours trying different things, reinstalling, trying to figure what lmtools does, etc. When I did try out lmtools it showed something about "Xilinx" in one of the status boxes, so that leads me to believe that perhaps Xilinx Vivado is also using FlexLM and that's why the installation failed, because FlexLM is already installed.
I uninstalled FLEXnet Publishing License Server Manager using the Control Panel-Add/Remove and restarted the PC, but when I check the Windows Services (via Task Manager) it sill shows the following two services in the list: "FLEXnet Licensing Service" and "FlexNet Licensing Service 64". When I look at the properties, it shows that the executables are in C:\Program Files (x86)\Common Files\Macrovision Shared\FLEXnet Publisher\FNPLicensingService64.exe.
I uninstalled Xilinx Vivado, checked Windows services but unfortunately the two FlexLM services still appear (though they are stopped). There is nothing in the Control Panel-Add/Remove Programs that is related to FlexNet
I have started the services (via the Windows Task Manager) and have tried opening a browser with localhost:8080 and 127.0.0.1:8080 and neither give anything back.
I've look on the Internet for ways to uninstall but they all say use Control Panel.
So...
a) any tips on how to get rid of the "other" FLEXnet install.
b) or, how do I use the existing FLEXnet install to also provide licensing for CCS (this is strangely omitted from TI's instructions) I would think that lmtools can be used to do this but I need instruction on to set up tidspssw this way.