I have CCS v 6.0.1.00040 and I need to configure network proxy settings. When I tell CCS to check for updates, everything seems to happen with no problem. But if I try to go to the Eclipse Marketplace it says proxy authentication is required.
So, I go to Window > Preferences > General > Network Connections, where I have schema for both HTTP and HTTPS configured with the correct Host and Port, but both says no authentication and there is no user and password. The problem is that after I add the user and password, clicking Apply, I can see them in the Network Connections, but when I click on OK to close the window and then I reopen the window the credentials have vanished. I am unable to go to the Eclipse Marketplace.
Strangely, when I first open CCS, it prompts me for proxy authentications credentials, and once I provide them it is happy.
Of course this is a bug. It would also be nice if, when going to the Eclipse Marketplace fails due to a lack of credentials, CCS would prompt me for the credentials right then and use them just as it does when I first open CCS.