Hi,
I am debugging Concerto M35 dual core code, but my question is broader:
In CCS, someone can always see expressions in one expression view. It is also possible to open second, third, etc. expression view, but ALL OF THEM SHOW THE SAME EXPRESSIONS. If expression is deleted from one view, it is deleted from all. Below is shown two "Expressions" and "Expressions(1)" tabs showing identical variables
Is it possible to assign DIFFERENT expressions to different "expressions" views (or per project, per core, etc),
like in MS Visual Studio, KEIL compiler, etc?
Below is a picture of MS Visual studio, when "Watch 1" window shows different variables than "Watch 2"