I am trying to convert a .out file to a .hex file to program this device. Everything I've read so far points to aquiring Code Composer Studio 3.3 in order to use dsphex to convert the file. Does hex2000 have the ability to do this? I tried using it in Windows 7 and it appeared to work. It showed up as an Intel hex in our programming software, however after programming the device the board didn't work. Maybe I need to set the romwidth to 16? The only thing I have available to work with is the customer's .out file.