Hi I'm trying to connect my computer using CCS to the MSP-EXP430FR5969 and I'm receiving the errors (1), followed by (2) below. I then tried to update the software, and clicked "check for updates" and received message (3). When I click ok, I receive error (4). I tried going to the url on firefox and it said (5). In addition, when I click on CCS App Center, a new tab opens up that's completely empty. I am running ubontu on on a Macintosh Air 84:38:35:5e:d8:92 I am pretty sure the issue stems from CCS needing to be updated. My research team Lead is using a macbook and he is able to connect to the same MSP. We are both using the same internet, which has a firewall setting of default.]
[Steps Needed to Recreate Problem:
1) Error initializing emulator: MSP-FET430UIF is already in use 2)Starting Debug Server ... MSP430: Error initializing emulator: MSP-FET430UIF is already in use 3)No updates were found. 4)No repository found at http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/uniflash. 5)File not found."