Sometimes when I start a debug session I get the error below. It happens sometimes and most of the time the debugger works fine. I usually have to try resetting the board and debug session until it starts to work again.
Using AM3359 ICE_V2 eval board with CCS 6.0.1
Error:
CortxA8: Trouble Writing Memory Block at 0x80000000 on Page 0 of Length 0xf4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0)
CortxA8: GEL: File: C:\Users\sdhunna\Documents\SIL\Software\IoModule\EcSlave\Debug\EcSlave.out: Load failed.
CortxA8: Unable to terminate memory download: NULL buffer pointer at 0x3a9f