I'm debugging a modified production application for the F2812 in CCVSv6.1.0.00104 that uses DSP/BIOS 5.42.1.09. I'm using an XDS-200 JTAG emulator. During single-stepping, sometimes CCS tries to launch a 2nd copy (process) of CCS for no apparent reason. It never quite fully starts though as it tells me my default work space is in use, so I usually close it. If I give it an alternate work space, it will fully open to the getting started page. At least most recently, it happened when the PC was pointing to cint00() at address 0x3da9f8, which is in flash.
This is very annoying and time consuming while I'm trying to debug a serious problem. What can I do to keep this from happening?
Thanks.