Hello All,
I am using Code Composer v6.1 on a Surface Pro 3 with Windows 10. So that means the icons are super tiny.
I know that because of the version of Eclipse that this version uses, there is nothing that can be done until we get CCS v7 near the end of the year but I believe that this messes with the way the Profile Clock is displayed.
When I debug, Choose Run>Clock>Enable, the Profile Clock isn't displayed correctly; only a sliver is displayed, so I cannot see the actual yellow clock or the numerical clock cycles.
It worked only once, but I moved it from the bottom status bar to the top toolbar and ever since I have not been able to see it. Is it possible to reset the icons or view/layout of Code Composer?
I've tried restarting CCS and even reinstalling CCS (I'm guessing some configuration file survived).
Any help is appreciated.
Thanks in advance.